CCID Command/Instruction Version

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CCID Command/Instruction Version

2,043 Views
sachin_singh
Contributor II

Hi, 

I am looking for the command/instruction version number used in phExCcid example "PN7462AU-FW_v05.07.01_Full" firmware example.

So, can you please help me to get the version number of CCID command/instruction used in firmware example.

Looking forward for the responses ... !

Regards

0 Kudos
Reply
1 Reply

1,949 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hello,

Please kindly refer to https://usb.org/sites/default/files/DWG_Smart-Card_CCID_Rev110.pdf  for details.

Hope that helps,

Have a great day,
Kan

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply