CAN initialization Failed (s12zvm)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CAN initialization Failed (s12zvm)

1,923 次查看
bijoykrishnasha
Contributor I

I am using  S12ZVM12EVB Evaluation Board (MC9S12ZVMC128MKH processor, No CAN PHY ,4MHz XTAL for CAN Bus). In CAN_init()  function controller hanged up  in exit initialisation mode , when it comes to  while loop.

pastedImage_2.png

No idea why? Any help will be appreciated....Thanks

0 项奖励
回复
2 回复数

1,801 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Bijoy krishna Sharma ,

Which CAN driver do you used ?

Your project is a demo code or created by yourself?

If you use CodeWarrior IDE,  you can first test create a project with Processor Expert,

there is example for CAN, test whether it can work well on your board.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,801 次查看
bijoykrishnasha
Contributor I

Hello Alice_Yang,

Thanks for your reply. In my Eval. Board (S12ZVM12EVB) i have no CAN Physical driver with the controller but an extra CAN PHY Driver is mounted in the Board. Yes, I used processor expert and the problem is solved.

Anyway thanks for you  advice.....Have a nice day.

BKS

0 项奖励
回复