No driver support in SDK Wizard for MKL17Z ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No driver support in SDK Wizard for MKL17Z ?

729 Views
geoff_s
Contributor III

I'm running the latest MCUXpresso IDE (v10.2.0).  I have built and installed current v2.4 SDK's for MKL17Z processors from the MCUXpresso SDK builder site. 

I'm trying to create a new project using the SDK Builder wizard, but when I get to the step where you select which drivers and middleware to include, the list of drivers is completely empty except for the clock driver.

Untitled.png

I'm sure I haven't had this issue before using older IDE/SDK versions, and the problem doesn't occur if I use a different processor from a similar family (eg KL16Z, KL27Z), or different processors entirely (eg KL28Z, K64F).

Is this just a bug with the IDE and/or SDK, or is the KL17Z no longer supported ?

0 Kudos
3 Replies

526 Views
danielchen
NXP TechSupport
NXP TechSupport

HI  geoff_s

Please download the latest SDK 2.4 packages from NXP website again. The old versions seems have problems. Now it has been fixed.

pastedImage_1.png

Regards

Daniel

0 Kudos

526 Views
norbertwitt
Contributor I

Hi,

I'm still missing the driver and also examples for DAC.

RegardsmissingDAC.jpg

0 Kudos

526 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Norbert Witt

There are two chips for KL27,  only one has 12-bit DAC.

For frdmkl27 board, no dac component.

If your chip has 12-bit DAC, you can use the DAC driver in KL43.

Regards

Daniel

0 Kudos