import

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

import

1,616件の閲覧回数
imrankhan
Contributor II

Hi Forum,

I am trying to import an SDK_2.2.0_MKL14Z32xxx4.mex file into  MCUXpresso IDE to use chipset device MKL14Z32VTF and create a project from the scratch. Since there is no near compatible board for the MKL14xx in the new project creation library. IS there any way one can suggest how can be imported the above file for correct pin muxing, clock etc?

Greatly appreciated. Thank you. 

ラベル(1)
0 件の賞賛
返信
1 返信

1,500件の閲覧回数
marek-trmac
NXP Employee
NXP Employee

Hi Imran,

it shall be possible to import configuration from existing MEX file into existing MCU IDE project using:

- right click on the project in Project Explorer and select import from popup menu

- select MCUXpresso Config Tools - Import Configuration (*.mex)

Hope this helps

Regards

Marek

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 件の賞賛
返信