import

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

import

1,629 Views
imrankhan
Contributor II

Hi Forum,

I am trying to import an SDK_2.2.0_MKL14Z32xxx4.mex file into  MCUXpresso IDE to use chipset device MKL14Z32VTF and create a project from the scratch. Since there is no near compatible board for the MKL14xx in the new project creation library. IS there any way one can suggest how can be imported the above file for correct pin muxing, clock etc?

Greatly appreciated. Thank you. 

Labels (1)
0 Kudos
Reply
1 Reply

1,513 Views
marek-trmac
NXP Employee
NXP Employee

Hi Imran,

it shall be possible to import configuration from existing MEX file into existing MCU IDE project using:

- right click on the project in Project Explorer and select import from popup menu

- select MCUXpresso Config Tools - Import Configuration (*.mex)

Hope this helps

Regards

Marek

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 Kudos
Reply