SCT/PWM configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SCT/PWM configuration

Jump to solution
3,082 Views
Deeps_bang
Contributor III

Hi Team,

I have to Cofigure SCTimer/PWM for my Application using MCUXpresso Configuration tools. How to do this ? what all parameters setting should be necessary while configuring for this SCT/PWM ?Any video link or Documentation would be really Appreciable.

Working Environment:

 Development board: LPC 55s69

SDK: SDK_2.x_LPC55s69

IDE: MCUXpresso V11.6.0

OS: Windows 10Pro

Thank you

Regards,

Deep_Bang

 

0 Kudos
Reply
1 Solution
3,039 Views
Petr_H
NXP Employee
NXP Employee

Hi, 

Recently, there was introduced a new register init component for SCTimer configuration and initialization. I recommend using this new component as it provides full capabilities of the SCTimer peripeheral and it generates a simpler code with lower memory footprint.

Petr_H_1-1667402460531.png

It also provides a set of presets for several basic use-cases that can be selected using the 'Preset' combo box in the SCT section. You can select some of these presets an then continue tweaking the individual settings :

Petr_H_2-1667402551023.png

If you are new to the SCTimer topic, it may be interesting for you to check the SCT cookbook available here .

Best regards

Petr Hradsky

Config Tools Team  

 

 

 

  

View solution in original post

0 Kudos
Reply
3 Replies
3,040 Views
Petr_H
NXP Employee
NXP Employee

Hi, 

Recently, there was introduced a new register init component for SCTimer configuration and initialization. I recommend using this new component as it provides full capabilities of the SCTimer peripeheral and it generates a simpler code with lower memory footprint.

Petr_H_1-1667402460531.png

It also provides a set of presets for several basic use-cases that can be selected using the 'Preset' combo box in the SCT section. You can select some of these presets an then continue tweaking the individual settings :

Petr_H_2-1667402551023.png

If you are new to the SCTimer topic, it may be interesting for you to check the SCT cookbook available here .

Best regards

Petr Hradsky

Config Tools Team  

 

 

 

  

0 Kudos
Reply
3,060 Views
Deeps_bang
Contributor III

oh ok Alice...

Thank you

0 Kudos
Reply
3,062 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Deep_Bang,

Sorry there is no such video or document. 

This configuration tool is easy to use, there is some reminders in every configurations, for example:

Alice_Yang_0-1667187482550.png

 

BR

Alice

0 Kudos
Reply