SCT/PWM configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SCT/PWM configuration

ソリューションへジャンプ
3,065件の閲覧回数
Deeps_bang
Contributor III

Hi Team,

I have to Cofigure SCTimer/PWM for my Application using MCUXpresso Configuration tools. How to do this ? what all parameters setting should be necessary while configuring for this SCT/PWM ?Any video link or Documentation would be really Appreciable.

Working Environment:

 Development board: LPC 55s69

SDK: SDK_2.x_LPC55s69

IDE: MCUXpresso V11.6.0

OS: Windows 10Pro

Thank you

Regards,

Deep_Bang

 

0 件の賞賛
返信
1 解決策
3,022件の閲覧回数
Petr_H
NXP Employee
NXP Employee

Hi, 

Recently, there was introduced a new register init component for SCTimer configuration and initialization. I recommend using this new component as it provides full capabilities of the SCTimer peripeheral and it generates a simpler code with lower memory footprint.

Petr_H_1-1667402460531.png

It also provides a set of presets for several basic use-cases that can be selected using the 'Preset' combo box in the SCT section. You can select some of these presets an then continue tweaking the individual settings :

Petr_H_2-1667402551023.png

If you are new to the SCTimer topic, it may be interesting for you to check the SCT cookbook available here .

Best regards

Petr Hradsky

Config Tools Team  

 

 

 

  

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,023件の閲覧回数
Petr_H
NXP Employee
NXP Employee

Hi, 

Recently, there was introduced a new register init component for SCTimer configuration and initialization. I recommend using this new component as it provides full capabilities of the SCTimer peripeheral and it generates a simpler code with lower memory footprint.

Petr_H_1-1667402460531.png

It also provides a set of presets for several basic use-cases that can be selected using the 'Preset' combo box in the SCT section. You can select some of these presets an then continue tweaking the individual settings :

Petr_H_2-1667402551023.png

If you are new to the SCTimer topic, it may be interesting for you to check the SCT cookbook available here .

Best regards

Petr Hradsky

Config Tools Team  

 

 

 

  

0 件の賞賛
返信
3,043件の閲覧回数
Deeps_bang
Contributor III

oh ok Alice...

Thank you

0 件の賞賛
返信
3,045件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Deep_Bang,

Sorry there is no such video or document. 

This configuration tool is easy to use, there is some reminders in every configurations, for example:

Alice_Yang_0-1667187482550.png

 

BR

Alice

0 件の賞賛
返信