Pin Mux Tools and Muxed ADC inputs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Pin Mux Tools and Muxed ADC inputs

3,495 次查看
bitjockey
Contributor II

New to the pin tool and was trying to configure a KV46 MCU's multiplexed ADC inputs (ADCA Channels 6 & 7) when I go to enable any one after the first , (ADCA_ch6a, b, c etc..) the check boxes for those muxed channels turn from green to being highlighted in red. When I hover over the red boxes it displays that the routing and the SIM_ADCOPT register is multiply defined, and warn about the Channel select for the ADC channel 6 and/or 7. I guess I was wondering if I can ignore this since I will be manually controlling the mux registers in software?

 

Regards,

标签 (1)
标记 (1)
3 回复数

3,081 次查看
BlackNight
NXP Employee
NXP Employee

Hi Brian,

you can ignore (if you want) warnings, but not errors in red. As long as there are errors, code is not generated/updated, so you have to resolve the errors.

pastedImage_1.png

You indicate that you are changing the muxing during runtime

For switching muxing at runtime you can create functions. For this you add a 'tab' in the routed pins view (you can give each tab its own name):

pastedImage_2.png

pastedImage_3.png

That way you can have both sub channels be configured, as they won't be active at the same time:

pastedImage_4.png

And you have two functions (named after the tabs) you can call for the muxing from your application:

pastedImage_5.png

I hope this helps,

Erich

0 项奖励
回复

3,081 次查看
pierre_garon
Contributor I

Hello Erich,

I am having the same problems has Brian. I tried your solution, however it does not work as my MCUXpresso configuration tool does not offer me the option of adding "tabs" to define sub-channels. Is there another way to do that? I am using MCUXpresso Config Tool version 5.0. My MCU is an MKV46F256VLL.

Thank you,

Pierre Garon.

0 项奖励
回复

3,082 次查看
marek-trmac
NXP Employee
NXP Employee

Hi guys,

in the latest version, tabs were replaced by functional groups, see tool bar.

For each functional group, one C-function will be generated.

Regards

Marek

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button