Pin Config Tools cell not align

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Pin Config Tools cell not align

3,346件の閲覧回数
phantomgz
Contributor IV

Hello,

Just have a look, will understand what I said. I am working with a 4K LCD screen, Windows10

 

168.png

0 件の賞賛
返信
3 返答(返信)

3,305件の閲覧回数
phantomgz
Contributor IV

Hi tomasklir,

No mater what I do that you have menention action, the same issue still exist.

I am working with :

Windows 10, 4K screen

MCUXpresso IDE v11.5.1 [Build 7266] [2022-04-13]

SDK_2_11_1_EVKB-IMXRT1050

167.png

0 件の賞賛
返信

3,280件の閲覧回数
tomasklir
NXP Employee
NXP Employee

Hi @phantomgz,
I sitll haven't managed to break it.
Have you tried to close the view and re-open it?
When you create a different configuration does the issue still persists? If not, could you share the configuration that breaks the view?
(EDIT: By sharing the configuration I mean the MEX file)

0 件の賞賛
返信

3,319件の閲覧回数
tomasklir
NXP Employee
NXP Employee

Hi @phantomgz,
whatever I do it's always aligned on my PC. I'll need more information...

Can you reproduce it? What is the scenario?

What version of Config tools are you using?

Is the alignment permanently broken or it get fixed for example after scrolling, switching tools, routing, etc?

0 件の賞賛
返信