Pin Config Tools cell not align

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pin Config Tools cell not align

3,364 Views
phantomgz
Contributor IV

Hello,

Just have a look, will understand what I said. I am working with a 4K LCD screen, Windows10

 

168.png

0 Kudos
Reply
3 Replies

3,323 Views
phantomgz
Contributor IV

Hi tomasklir,

No mater what I do that you have menention action, the same issue still exist.

I am working with :

Windows 10, 4K screen

MCUXpresso IDE v11.5.1 [Build 7266] [2022-04-13]

SDK_2_11_1_EVKB-IMXRT1050

167.png

0 Kudos
Reply

3,298 Views
tomasklir
NXP Employee
NXP Employee

Hi @phantomgz,
I sitll haven't managed to break it.
Have you tried to close the view and re-open it?
When you create a different configuration does the issue still persists? If not, could you share the configuration that breaks the view?
(EDIT: By sharing the configuration I mean the MEX file)

0 Kudos
Reply

3,337 Views
tomasklir
NXP Employee
NXP Employee

Hi @phantomgz,
whatever I do it's always aligned on my PC. I'll need more information...

Can you reproduce it? What is the scenario?

What version of Config tools are you using?

Is the alignment permanently broken or it get fixed for example after scrolling, switching tools, routing, etc?

0 Kudos
Reply