MCUXpresso Pin ConfigTools Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpresso Pin ConfigTools Error

ソリューションへジャンプ
3,569件の閲覧回数
hamed
Contributor I

Hi all,

I am trying to use pin config tool in MCUXpresso with my MKE04Z128VQH4 MCU. The problem is when I enable the SWD CLK and DIO pins, it doesn't let me enable FTM1-CH0 on pin 6. There seem to be no conflict by looking at the datasheet, but it tells me there is conflict in setting SWDE bit of SIM_SOPT0 register. Your help is appreciated.

ラベル(1)
0 件の賞賛
返信
1 解決策
3,388件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Hamed Mohammadi,

There seem to be no conflict.
In fact you don't need to enable SWD CLK and DIO pins, these two pins are default as these function.

SWD.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
3,389件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Hamed Mohammadi,

There seem to be no conflict.
In fact you don't need to enable SWD CLK and DIO pins, these two pins are default as these function.

SWD.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,388件の閲覧回数
hamed
Contributor I

Thanks!

0 件の賞賛
返信