MCUXpresso IDE v10.2.0 [Build 759] : can't use config tool for K64F : MK64FN1M0VMD12

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso IDE v10.2.0 [Build 759] : can't use config tool for K64F : MK64FN1M0VMD12

Jump to solution
5,555 Views
jean-francoisau
NXP Employee
NXP Employee

Hi all,

When I use MCUXpresso IDE v10.1.1 [Build 606] [2018-01-02],

   Create a new project :

 select    frdmk64f,

SDK_2.x_FRDM-K64F, (2.3.0)

Device packages: MK64FN1M0VMD12

   Open MCUxpresso config tool:

               By default the selected package is MK64FN1M0VLL12….

               Even if I chose MK64FN1M0VMD12 during le project creation…

                But I can switch package from MCUxpresso config tool

                It works fine !

        

 

When I use MCUXpresso IDE v10.2.0 [Build 759] [2018-05-15],

           

            Create a new project :

    select    frdmk64f,

SDK_2.x_FRDM-K64F, (2.3.0)

Device packages: MK64FN1M0VMD12

Open MCUxpresso config tool:

 

               I receive the message from Config Tools Overview : The tool does not support selected processor

               When I try to switch Package, the list is empty…  

              

Could you help?

Best regards.JF

Tags (1)
1 Solution
4,986 Views
choppad
Contributor II

Hello Jean-Francois Aupee:

You will need to have an active network connection or if you need to work offline with any of the processors, you can do so by "Downloading Processor Data" from within MCUXpresso while you have an active connection.  You can find details on how to accomplish this in the  "MCUXpresso ConfigTools User Manual - Section 6.3".  It can be found in your installation directory for MCUXpresso-> c:/nxp/MCUXpressoIDE_10.2.0_759 or download here -> MCUXpresso Config Tools User's Guide 

Finally, for your convenience, please find it attached.

Hope it Helps!

DeWayne 

View solution in original post

0 Kudos
Reply
8 Replies
4,985 Views
marek-trmac
NXP Employee
NXP Employee

Hi JF,

I tried to reproduce the problem and I've got different error message, saying: Part number "..VMD12" detected in MCU IDE project does not match with currently selected "...VLL12". This means you selected VMD12 in MCU IDE project settings but the project source code contains configuration for ...VLL12, which is used on FRDM-K64F.

To synchronize Config tools configuration with MCU IDE project, right-click on the error message and select quick fix: Switch to part-number: ...VMD12.

If this does not solve your problem, can you post a print screen with the error message? Otherwise please click the Correct Answer button.

Regards

Marek

Regards,
Marek


NOTE: If you find the answer useful, kindly click on "ACCEPT AS SOLUTION" button
0 Kudos
Reply
4,986 Views
jean-francoisau
NXP Employee
NXP Employee

Hi Marek,

Yes I use the switch package too.

Regards

JF

0 Kudos
Reply
4,986 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello  Jean-francois Aupee ,

Please download and install the new SDKv2.4 into  MCUXpresso IDE v10.2:

https://mcuxpresso.nxp.com/en/builder    

Hope it helps,


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
4,986 Views
jean-francoisau
NXP Employee
NXP Employee

Hi Alice,

I had already tried but didn't solve the problem...

But you're right it is better to use this version..

Thanks

JF

0 Kudos
Reply
4,987 Views
choppad
Contributor II

Hello Jean-Francois Aupee:

You will need to have an active network connection or if you need to work offline with any of the processors, you can do so by "Downloading Processor Data" from within MCUXpresso while you have an active connection.  You can find details on how to accomplish this in the  "MCUXpresso ConfigTools User Manual - Section 6.3".  It can be found in your installation directory for MCUXpresso-> c:/nxp/MCUXpressoIDE_10.2.0_759 or download here -> MCUXpresso Config Tools User's Guide 

Finally, for your convenience, please find it attached.

Hope it Helps!

DeWayne 

0 Kudos
Reply
4,986 Views
jean-francoisau
NXP Employee
NXP Employee

Hi DeWayne,

Thanks a lot it solves the issue !

Regards

JF

4,986 Views
choppad
Contributor II

You bet Sir!

DeWayne

4,986 Views
jean-francoisau
NXP Employee
NXP Employee

;)

JF

0 Kudos
Reply