MCUXpresso Config Tools eclipse project file not generated

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpresso Config Tools eclipse project file not generated

3,732件の閲覧回数
yusufhusainy
Contributor I

Hi All,

 

On creating a new MKW41Z configuration or using an existing one from the SDK examples, the '.cproject' file and other files required by the eclipse based MCUXpresso IDE do not get generated. The source files that do get generated are board, startup and application main.c, besides that, the selected driver files in the 'Project Configuration' view of the Config tools do not get copied in to the destination project path.

 

The tools version are as follows on my PC:

MCUXpresso IDE:"MCUXpresso IDE v10.0.0 [Build 344] [2017-03-21] "

MCUXpresso Config Tools: Version 3.0

MK41Z SDK:SDK_2.2_FRDM-KW41Z

 

See attached '.mex' file.

 

Any Help is appreciated!

 

Regards,

Yusuf Husainy.

Original Attachment has been moved to: WiiUartBm.mex.zip

タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,598件の閲覧回数
marek-trmac
NXP Employee
NXP Employee

Hi again,

Here is the step-by-step procedure copied from the documentation:

To open a generated project in the MCUXpresso IDE:

  1. Start the MCUXpresso IDE.
  2. Open Installed SDKs view and ensure that the SDK is installed.
  3. Navigate to the Quickstart Panel view and select Import SDK example(s)….
  4. Select SDK and click Next.
  5. Click the Import from XML… button on the toolbar.
  6. Select the generated XML file
  7. In the list of examples, expand the Project Generator category and select the generated example.
  8. Confirm to import.

Regards, Marek

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 件の賞賛
返信

2,598件の閲覧回数
marek-trmac
NXP Employee
NXP Employee

Hi Yusuf Husainy,

for MCUXpresso IDE, there is generated 'xml' project file instead of native project file. Please follow documentation to import project into MCUXpresso IDE.

Regards

Marek 

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 件の賞賛
返信