LPC55S69 - GPIO Pin as NMI using Config Tools

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S69 - GPIO Pin as NMI using Config Tools

ソリューションへジャンプ
4,072件の閲覧回数
PhilV
Contributor III

Hi, I am using mcuXpresso with the config tool to setup an LPC55S69.

I want PIO1_18 to be non-maskable-interrupt.
In the user manual for the LPC55S69 it seems to indicate that this is possible, but I do not see how to do this via the configuration tools?

In the Pin Configuration "Pins" table I have set it for "PINT:PINT,0" (do I also need to set it as GPIO?)

In the Peripherals Configuration tool I can then configure the PINT for Falling edge etc.
I can also choose to "Enable callback/interrupt" - (what is the reason for being able to configure it and not enable it?)
If I enable it I can then name a callback function and handle it... but I don't see any option to make this the NMI? 

Please advise?

0 件の賞賛
返信
1 解決策
4,043件の閲覧回数
Miguel04
NXP TechSupport
NXP TechSupport

Hi @PhilV 

Config tools is usefull for some "simple" configurations and it does not supports all the modules, since the SYSCON is something more complicated besides the clocks configurations and the NMI setup has to be by writing on the register by programming them.

Best Regards, Miguel.

元の投稿で解決策を見る

2 返答(返信)
3,947件の閲覧回数
PhilV
Contributor III

Just for future visitors... 

See also this thread for the implementation details:

https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-IRQ-Numbers-for-NMI/m-p/1723892/highlight...

4,044件の閲覧回数
Miguel04
NXP TechSupport
NXP TechSupport

Hi @PhilV 

Config tools is usefull for some "simple" configurations and it does not supports all the modules, since the SYSCON is something more complicated besides the clocks configurations and the NMI setup has to be by writing on the register by programming them.

Best Regards, Miguel.