Is the EDMA Auto stop request initialization missing?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is the EDMA Auto stop request initialization missing?

跳至解决方案
5,922 次查看
imxrtuser
Senior Contributor I

Hello jch

unfortunately I had some more troubles when using ADC and DMA.

The setting Auto stop request

pastedImage_5.png

only results in code when enabling the checkbox.

If I do not enable it I assume that it is disabled, but the reference manual shows that the DREQ bit

pastedImage_6.png

is unkonw after reset. In my test cases it always was set to '1' after reset which was not what I wanted it to be when running my code which I set up with MCUXpresso Config Tools.

I think MCUXpresso Config Tools should always include the line

 EDMA_EnableAutoStopRequest(DMA_BASEADDR, USED_DMA_CHANNEL, false);

and set it to true if the checkbox is enabled.

Do you think this makes sense to get included in the next MCUXpresso Config Tools build?

Kind regards,

Stefan

标记 (2)
0 项奖励
回复
1 解答
5,780 次查看
martin_stano
NXP Employee
NXP Employee

Hi,

thank you for your feedback and the detailed describtion. I analyzed the problem and now I realized that the default initialized state of the TCD is as you described above. I will prepare the update of the component.

Best Regards,

Martin

在原帖中查看解决方案

0 项奖励
回复
6 回复数
5,777 次查看
martin_stano
NXP Employee
NXP Employee

Hi Stefan,

in the following attachment there is a hotfix for your issue. There is information how to install the patch in the package.

Best Regards 

Martin

5,777 次查看
imxrtuser
Senior Contributor I

Thank you Martin!

Do you know when the next SDK version which includes all hotfixes will be released?

Kind regards,

Stefan

0 项奖励
回复
5,777 次查看
martin_stano
NXP Employee
NXP Employee

Hi,

regarding your issue description, there might be a problem, that you have not called EDMA_ResetChannel() function which will set DREQ (in the component enable Reset channel setting). Please, test it and let me know if the problem remains.

Best Regards

Martin

0 项奖励
回复
5,777 次查看
imxrtuser
Senior Contributor I

Hello,

thank you for the hint. The function EDMA_ResetChannel gets called (checkbox active) and therefore the DREQ bit gets set to 1.

If I use the checkbox "Reset channel" (which I think is good because the peripheral will be set to a known state) I have no way to disable the Auto stop request in MCUXpresso Config tools even if the checkbox "Auto stop request" looks like I have disabled the auto stop feature. If I do not set the checkbox Auto stop request no code will be generated and therefore the DREQ bit will stay at 1 until I call

EDMA_EnableAutoStopRequest(DMA0_DMA_BASEADDR, DMA0_CH0_DMA_CHANNEL, false);

in my own source code.

Kind regards,

Stefan

0 项奖励
回复
5,781 次查看
martin_stano
NXP Employee
NXP Employee

Hi,

thank you for your feedback and the detailed describtion. I analyzed the problem and now I realized that the default initialized state of the TCD is as you described above. I will prepare the update of the component.

Best Regards,

Martin

0 项奖励
回复
5,777 次查看
jch
NXP Employee
NXP Employee

Hi Stefan, 

I think that better person for this is martinstano.

Hi Martin, can you please look at it?

Thanks a lot

Jiri

0 项奖励
回复