How to use the Memory Validation Tool in MCUXpresso Config Tools?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use the Memory Validation Tool in MCUXpresso Config Tools?

1,434 Views
Raymond_Yang
Contributor II

Hello,

In the release note of MCUXpresso Config Tools, it has the following info for Memory Validation tool, but I can't find where to launch this tool from the Config Tools IDE. Also, in the user guide GSMCUXCTUG.pdf, it doesn't mention anything about this tool. That's confusing. Please confirm.

 

Memory Validation tool
=========================
The Memory Validation tool allows testing of SEMC, FlexSPI and FCB configuration by running different
scenarios on board
- Support for SEMC registers init component
- Support for FlexSPI register init component
- Support for FCB
- Added FlexSPI transaction blocking test
- Added custom test containing multiple configurable FlexSPI transactions

Tags (1)
0 Kudos
Reply
4 Replies

1,304 Views
Raymond_Yang
Contributor II

Take FLEXSPI as example, where is the button to open memory validation tool?

Raymond_Yang_0-1747573608596.png

 

 

0 Kudos
Reply

1,272 Views
addiyi
NXP Employee
NXP Employee
Hi,

For FlexSPI please use the Register Initialization component, not the Peripheral component.

Adrian
0 Kudos
Reply

1,170 Views
Raymond_Yang
Contributor II

Thanks. I can find it now.

0 Kudos
Reply

1,387 Views
addiyi
NXP Employee
NXP Employee

Hi,

The Memory validation feature is available on top of Peripherals tool, for Register initialization component SEMC and FLEXSPI and for Peripheral device FCB.

Once one of above is opened you will find the button to open the Validation View on top right of the component window. The In Validation window you'll find all the supported tests and the test options. 

The tests are executed using the configuration you do in the UI.

 

Adrian

0 Kudos
Reply