Error!!!: Could not determine GDB version using command: gdb --version

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error!!!: Could not determine GDB version using command: gdb --version

3,304 Views
kpki
Contributor I

Error!!!: Could not determine GDB version using command: gdb --version

pastedImage_1.png

I get this above error while trying to debug an application which is compiled to run on X86 platform (windows 10).

The application works in 'run mode' but when launched in 'Debug mode' this error comes. Below is the version details of my MCUXpresso.

pastedImage_2.png

Is there any solution for the same? I have a cygwin compiler on the windows 10 PC. When i run the gdb --version in my windows terminal it correctly prints the gdb version as shown below.

pastedImage_3.png

Please helpout

0 Kudos
Reply
2 Replies

3,141 Views
marek-trmac
NXP Employee
NXP Employee

Hi Kiran,

this is a link to MCU IDE specific community: https://community.nxp.com/community/mcuxpresso/mcuxpresso-ide .

This community is intended for Configurations tools: Pins tool, Clocks tool, Peripherals tool, DCD tool and TEE tool.

Best Regards
Marek

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 Kudos
Reply

3,141 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello kpki‌,

This error in previous IDE versions was due to a problem with the paths from the debug session. Could you try installing the latest IDE version MCUXpresso 11.1.0 (check the link here) to see if this solves the issue?

Best Regards,

Alexis Andalon

0 Kudos
Reply