Standalone config tools v7.0 fails installation under Mac OS 10.15 (Catalina)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Standalone config tools v7.0 fails installation under Mac OS 10.15 (Catalina)

ソリューションへジャンプ
1,999件の閲覧回数
ernest1
Contributor I

I was excited to see v7.0 of the stand alone config tools finally released, however the installation still fails under MacOS 10.15 (Catalina) with the following message:

This package is incompatible with this version of macOS.

The package is trying to install content to the system volume. Contact the software manufacturer for assistance.

Is there any ETA for when the installer will be fixed? Thanks a lot in advance.

タグ(3)
1 解決策
1,849件の閲覧回数
liborukropec
NXP Employee
NXP Employee

Hello,

these days Config Tools version 7.0.1 were released which can be installed on Mac OS Catalina. Exception has to be added, as the installer is not notarized yet.

MCUXpresso Config Tools|Software Development for NXP Microcontrollers (MCUs) | NXP 

Regards,

Libor

元の投稿で解決策を見る

2 返答(返信)
1,850件の閲覧回数
liborukropec
NXP Employee
NXP Employee

Hello,

these days Config Tools version 7.0.1 were released which can be installed on Mac OS Catalina. Exception has to be added, as the installer is not notarized yet.

MCUXpresso Config Tools|Software Development for NXP Microcontrollers (MCUs) | NXP 

Regards,

Libor

1,849件の閲覧回数
liborukropec
NXP Employee
NXP Employee

Hello Ernesto,

 

we are aware of the issue and we are working on it, including the notarization process. I'll let you know once there's an outlook when the installer can be published.

 

Regards,

Libor

0 件の賞賛
返信