Configuring LPC54606's SDIF Interface Using MCUXpresso Config Tools

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configuring LPC54606's SDIF Interface Using MCUXpresso Config Tools

1,705 Views
Gu01
Contributor I

Hi,

I am using the LPC54606J512BD100 MCU and need to connect an eMMC chip. However, I have found that MCUXpresso Config Tools V13.1 does not have an option to configure the SDIF module. The clock frequency is set to 180MHz, and the SDIO clock has been enabled. The corresponding SDIF ports are also configured. Is there any way to initialize the SDIF module configuration using MCUXpresso Config Tools?

Thanks!

0 Kudos
Reply
1 Reply

1,678 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Gu01 

Yes, the config tool doesn't support this module. There is demos under SDK, you can refer to:

Alice_Yang_0-1681116002625.pngAlice_Yang_0-1681116002625.png

 

BR

Alice

 

 

 

0 Kudos
Reply