Configuring LPC54606's SDIF Interface Using MCUXpresso Config Tools

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Configuring LPC54606's SDIF Interface Using MCUXpresso Config Tools

1,762 次查看
Gu01
Contributor I

Hi,

I am using the LPC54606J512BD100 MCU and need to connect an eMMC chip. However, I have found that MCUXpresso Config Tools V13.1 does not have an option to configure the SDIF module. The clock frequency is set to 180MHz, and the SDIO clock has been enabled. The corresponding SDIF ports are also configured. Is there any way to initialize the SDIF module configuration using MCUXpresso Config Tools?

Thanks!

0 项奖励
回复
1 回复

1,735 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Gu01 

Yes, the config tool doesn't support this module. There is demos under SDK, you can refer to:

Alice_Yang_0-1681116002625.png

 

BR

Alice

 

 

 

0 项奖励
回复