Configuring LPC54606's SDIF Interface Using MCUXpresso Config Tools

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Configuring LPC54606's SDIF Interface Using MCUXpresso Config Tools

1,701件の閲覧回数
Gu01
Contributor I

Hi,

I am using the LPC54606J512BD100 MCU and need to connect an eMMC chip. However, I have found that MCUXpresso Config Tools V13.1 does not have an option to configure the SDIF module. The clock frequency is set to 180MHz, and the SDIO clock has been enabled. The corresponding SDIF ports are also configured. Is there any way to initialize the SDIF module configuration using MCUXpresso Config Tools?

Thanks!

0 件の賞賛
返信
1 返信

1,674件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Gu01 

Yes, the config tool doesn't support this module. There is demos under SDK, you can refer to:

Alice_Yang_0-1681116002625.pngAlice_Yang_0-1681116002625.png

 

BR

Alice

 

 

 

0 件の賞賛
返信