Config_Tool_Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
6,082件の閲覧回数
farha
Contributor I

I  am facing issue. pin_mux.c  is not generating when i am doing pin configuration in Mcuxpresso config tool.

Pls help

0 件の賞賛
返信
1 解決策
6,066件の閲覧回数
Petr_H
NXP Employee
NXP Employee

Hi,

We need more information on what MCU are you using, what version of config tools and what steps have you done and if there is some error reported in the problems view. It would be also ideal if you could share the .mex file with the configuration so we can reproduce the problem.

Regards

Petr Hradsky

Config Tools Team

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
6,067件の閲覧回数
Petr_H
NXP Employee
NXP Employee

Hi,

We need more information on what MCU are you using, what version of config tools and what steps have you done and if there is some error reported in the problems view. It would be also ideal if you could share the .mex file with the configuration so we can reproduce the problem.

Regards

Petr Hradsky

Config Tools Team

0 件の賞賛
返信
6,055件の閲覧回数
farha
Contributor I

Hello,

Kindly check  my attachment docs. I have shared a .mex file .

Details:

IDE: MCUXpresso IDE v11.5.1_7266.

SDK: SDK_2.X_LPC54606J512.

Controller: LPC54606512.

 

 

 
0 件の賞賛
返信
6,016件の閲覧回数
Petr_H
NXP Employee
NXP Employee

Hi,

I'm sorry, I haven't been able to reproduce the problem with 'Internal error'.

However, the warnings that are shown in the tooltip "Device configuration is not supported..." only mean that these tools are not available because they require DCD and TrustZone modules that are not present on the LPC54606 microcotrollers. You can just ignore those warnings.

Does the problem with the "Internal error" message persist and is it always reproducible? 

If so, could you please send me the log file that is located in the following folder:

c:\Users\{your user id}\.nxp\nxp_conf_workspace_v11.0\.metadata\.log

Regards

Petr Hradsky

Config Tools Team