To use KinetisFlashTool application, is OPENSDA interface mandatory?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

To use KinetisFlashTool application, is OPENSDA interface mandatory?

2,632件の閲覧回数
srinivasa_raow
Contributor I

Hi,

 

I have TWR-K21F120MA. 

 

This board is having “OSBDM/OSJTAG” interface.

 

I am trying to follow the steps as explained in “Kinetis Bootloader Demo Application User's Guide” (Document Number: KBTLDRDEMOUG).

 

Since our board does not support OPENSDA, can we use KinetisFlashTool application with TWR-K21F120MA?

I am not able to establish connection with TWR-K21F120MA from KinetisFlashTool application and proceed further.

 

Or

 

To use KinetisFlashTool application, is OPENSDA interface mandatory?

 

Regards

Srinivasa

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,396件の閲覧回数
ramboyang
NXP Employee
NXP Employee

Hi, Srinivasa, no such limitation. Please feel free to use it with any standard UART ports.

Best Regards,

Fan

0 件の賞賛
返信

2,396件の閲覧回数
srinivasa_raow
Contributor I

Hi Fan,

Thanks for reply.

We are trying to follow the steps as mentioned in document “Getting Started with the Kinetis Flashloader (Document Number: KFLLDRUG)”.  

As explained in “3.2 The host utility application - blhost”, we are not able to establish connection with K21 board.

We have PC recognizing the device is OSJTAG on COM9 but unable to send any commands

Are we missing anything?

Regards

Srinivasa

0 件の賞賛
返信

2,396件の閲覧回数
ramboyang
NXP Employee
NXP Employee

Hi Srinivasa,

I just observed that you may try to use the pre-programmed Flashloader, right?

If so, please ensure that the device is just with factory settings, and it is the first time for you to communicate the device with host tool. If you have erased the flash with debugging tool such as OSJTAG, the flashloader would have been erased.

Thanks,

Fan

0 件の賞賛
返信