S32K144 bootloader CAN and/or UART2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 bootloader CAN and/or UART2

2,202 Views
filippo_malleo
Contributor I

Hi, 
I would need a bootloader code (or the rbf file) for the S32K144 MCU which works with CAN or UART2 (unfortunately I cannot use UART1, which is the only one used and working with RAppID Tool). 

Is there an rbf file which is configured to use CAN communication or UART2? 

Thanks and kind regards,
Filippo

0 Kudos
Reply
0 Replies