LPC4074 access on chip flash write/read

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4074 access on chip flash write/read

2,355件の閲覧回数
Jackson7781
Contributor I

 

スポイラ
Hi everyone. 
I'm new, I'm recently working on a Lpc4074 project, I want to  access flash for bootloader  application, is there any related resource that I can implement this  ?

thank you very much



 

0 件の賞賛
返信
1 返信

2,341件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Jackson7781 

The on board boot rom code is never open to external.

If you want to develop your own secondary bootloader, we don't have exact demo for LPC4074, but you can refer  it as well.

SPI secondary boot loader
https://www.nxp.com/docs/en/application-note/AN11257.zip

I2C secondary boot loader
https://www.nxp.com/docs/en/application-note/AN11258.zip

LPC1700 secondary USB bootloader
https://www.nxp.com/docs/en/application-note/AN10866.zip

These ANs are based on LPC17xx but motherd is the same for LPC40xx


This AN is Migrating from the LPC177x/8x to LPC407x/8x, in case you need it.
https://www.nxp.com/docs/en/application-note/AN11335.zip

 

Thanks,

Jun Zhang

0 件の賞賛
返信