Conditions for disabling time-out detection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Conditions for disabling time-out detection

ソリューションへジャンプ
2,500件の閲覧回数
masahirokiniwa
Contributor IV

Could you tell me conditions for disabling time-out, when I use KL03 ROM bootloader.

When boot-pin is asserted or user-application is not valided, ROM bootloader disable time-out detection.
It's wrote at KL03 reference manual Rev.4 P.113 Figure 11-2.
But ROM bootloader disabled time-out detection at another situation, when I ran it from my user application.

I ran bootloader by below sequence same as RM P.114 11.3.5.
// Read the function address from the ROM API tree.
runBootloaderAddress = **(uint32_t **)(0x1c00001c);
runBootloader = (void (*)(void * arg))runBootloaderAddress;
// Start the bootloader.
runBootloader(NULL);

And I set BCA as below.
tag = "kcfg"
enabledPeripherals = use only I2C
i2cSlaveAddress = 0x50
peripheralDetectionTimeout = 10000 (10s)

Could you tell me what happened for disabling time-out.

0 件の賞賛
返信
1 解決策
2,221件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Masahiro,

if you call the bootloader explicitly from your application, there is no timeout. So if you call the bootloader from your application, it stays in the bootloader until you do a reset.

Timeout is only used if bootloader is entered automatically after reset.

See other details in Getting Started: ROM Bootloader on the NXP FRDM-KL03Z Board | MCU on Eclipse .

I hope this helps,

Erich

元の投稿で解決策を見る

2 返答(返信)
2,222件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Masahiro,

if you call the bootloader explicitly from your application, there is no timeout. So if you call the bootloader from your application, it stays in the bootloader until you do a reset.

Timeout is only used if bootloader is entered automatically after reset.

See other details in Getting Started: ROM Bootloader on the NXP FRDM-KL03Z Board | MCU on Eclipse .

I hope this helps,

Erich

2,221件の閲覧回数
masahirokiniwa
Contributor IV

Hi Erich

Thank you for your answer.

I saw a reason of this case.

.

Best regards,

M.Kiniwa

0 件の賞賛
返信