Bootloader CRC (via BCA)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bootloader CRC (via BCA)

8,146 Views
jan_ymanas
Contributor II

Hi, 

We're working witch a Kinetis MKE18F with BootRom and want to check if the image was loaded correctly using the BCAs CRC. 

We tried to upload image via CANbus with our own application but we don't have any response about CRC status. After sending the valid or invalid (CRC corrupted) image, the bootloader only sends the GenericResponse with status code kStatus_Success from the WriteMemory command.

These are the CANbus frames received of this response:

TimeCAN IDLengthData
0026833197us 0x123 8    5A A4 0C 00 23 72 A0 00
0026833704us 0x123 8    00 02 00 00 00 00 04 00 
0026833980us 0x123 2    00 00

We tried it again with the KinetisFlashTool app via UART and the result was the same, wether setting the CRC configuration or not, we receive the same result (no feedback from the bootloader about the CRC application integrity testing)

We don't know how to get it working.

We followed the steps of chapter 23.7, Kinetis KE1xF Sub-Family Reference Manual:

pastedImage_1.png

But were should we receive these kStatus? When? After last data frame? Automatically? We don't have a clue.

In BCA we've configured the next CRC values:

.crcStartAddress = 0x000003d0, //!< Disable CRC check
 .crcByteCount = 0x000337fc, //!< Disable CRC check
 .crcExpectedValue = 0xF913CCAD, //!< Disable CRC check‍‍‍

Can you help us? 

Thank you so much! Smiley Happy

Labels (1)
10 Replies

7,827 Views
jan_ymanas
Contributor II

Hi all, :smileyhappy:

Thank you all for the replies, ErichS‌ , jayheng‌ and nxf46116. 

Mixing your replies and the reference manuals we got the right way to calculate CRC and apply it. We load the image (.bin) via CANbus and finishes with a reset, then the application start running. So, the process was successful.

But we still don't receiving the CRC kStatus, we don't have any information about CRC via CANbus. The PTA11 pin works and is or isn't asserted, depends if the CRC verification was successful or not.

Best regards,

Jan. 

0 Kudos
Reply

7,827 Views
jay_heng
NXP Employee
NXP Employee

For the image CRC32 calculation, You can use this online tool http://www.sunshine2k.de/coding/javascript/crc/crc_js.html with below configuration

 pastedImage_1.png

In Kinetis device, we need to bypass byte address 0x3cc ~ 0x3cf (bypass length is 4 byte) when calculating image CRC.

7,827 Views
jay_heng
NXP Employee
NXP Employee

The CRC32 algo is as below:

x32+x26+x23+x22+x16+x12+x11+x10+x8+x7+x5+x4+x2+x+1

pastedImage_1.png

0 Kudos
Reply

7,827 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello Jan,

For his you will first need to set the MCU to boot from ROM, with this after the reset the BCA configurations should be executed.

For this you need to set the FOPT, BOOTSRC_SEL first.

pastedImage_1.png

If you're using MCUXpresso, you can set this field writing in the startup code, in the flash config:

pastedImage_2.png

Let me know if this helps you.

Best Regards,

Alexis Andalon

0 Kudos
Reply

7,827 Views
jan_ymanas
Contributor II

Hi Alexis, 

thank you for replying. 

We already had this configuration to update via Bootloader:

FOPT-->

pastedImage_1.png

BCA-->

pastedImage_2.png

Everything goes alright until the host finishes writing the data to the target successfully and then we try to do a reset (5A A4 02 00 66 64 0B 00); after the reset the MCU is still in bootloader and does not exit by timeout.

But were should we receive the CRC kStatus? When? After the last data frame? We still don't have a clue.

Thanks :smileyhappy:

0 Kudos
Reply

7,827 Views
ErichStyger
Specialist I

This might be helpful too:

I'm using srec_cat to calculate the CRC, see Tutorial: CRC32 Checksum with the KBOOT Bootloader | MCU on Eclipse 

I hope this helps,

Erich

7,827 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello Jan,

As you mention, I also can't identify where this response is send, I will investigate further about this issue, but meanwhile if you want to identify if the CRC was done correctly the pin PTA 11 is asserted when the CRC check fail after the reset.

Best Regards,

Alexis Andalon

0 Kudos
Reply

7,827 Views
jan_ymanas
Contributor II

Thanks Alexis,

We keep trying too.

I think the pin PTA11 is asserted when CRC doesn't correct or Byte count is out of range, that's right? we'll try on a TWR board over the coming days. 

Otherwise, how the ROM Bootloader calculates the CRC? I mean, maybe we don't calculate the CRC correctly.

Thanks! :smileyhappy: Regards,

Jan.

0 Kudos
Reply

7,827 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello Jan,

I will suggest to check the Kinetis Bootloader  v2.0.0 Reference Manual in the chapter 4.5, you can find the algorithm to calculate the CRC, also if you want to compare I will suggest to use the KinetisFlashTool that you can find in the following link.

You will find it in the next path: NXP_Kinetis_Bootloader_2_0_0\bin\Tools\KinetisFlashTool\win, this tool can help you set the BCA configuration.

Best Regards,

Alexis Andalon

7,829 Views
jan_ymanas
Contributor II

Hi Alexis,

Thank you for reply!

In the chapter that you mentioned I see the CRC 16 algorithm (XMODEM variant) used for calculate the CRC for bootloader frames , but for CRC 32 algorithm (used by the Bootloader to check API integrity, 0x3CC) what is the variant that its uses? 

We noticed that in the 1.2.0 version of MCU Bootloader Reference Manual doesn't say anything about CRC 32 algorithm calculate but in 2.0.0 or 2.5.0 says CRC 32 uses MPEG2 algorithm variant. 

We have compared our CRC 32, standard and MPEG2, calculated value with the KFT value and doesn't match.

Our CRC 32 calculate:

pastedImage_2.png

KFT CRC 32 Calculate:

pastedImage_3.png

Best regards,

Jan.

0 Kudos
Reply