AN4368 AN4379 difference

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AN4368 AN4379 difference

Jump to solution
6,450 Views
pietrodicastri
Senior Contributor II

Good morning

I have the 2 application notes. Do they present the same thing?

The source code of the USB bootloader is now attached to the SDK as an option. Is it correct?

Just to know

Thank You

Pietro

1 Solution
6,193 Views
FelipeGarcia
NXP Employee
NXP Employee

Hello Pietro,

 

I am very sorry for my late reply. We have been under a big workload and we have many questions on the queue.

 

Unfortunately, in in mcu-boot for FRDM-K64F there is no MSD bootloader example. However, I recommend you to check the community document below. This bootloader was implemented for IAR IDE.

 

https://community.nxp.com/docs/DOC-102629 

 

If you want to learn more about MCUXpresso IDE I recommend you to watch the following videos.

 

MCUXpresso IDE - Introduction Video

MCUXpresso IDE - Importing SDK Libraries

MCUXpresso IDE - Creating a new SDK Project

MCUXpresso IDE - Importing an SDK Example Project

MCUXpresso IDE - Using LPCOpen Examples

MCUXpresso IDE - Project Settings

 

Hope it helps!

 

Best regards,

Felipe

View solution in original post

11 Replies
6,193 Views
pietrodicastri
Senior Contributor II

Hello Felipe

Justg give me a signal.

I would like to have a help to understand the way MCUXpresso is doing.

And suggestion to use this application to get a bootloader without digging too much

in USB details.

The Derek solution tris to discriminate the writing to the  disk with the sector number, in his case is

FATDataSec0 = 520

I have seen trying to drop a file of 1KB the sector number is 43.

If someone with a qualified exoerience in the USB mass storage in reachable I would like to hear from.

If I can deterministically know what is the sector data number for the data, starting from the initialization of the disk size,

I think I can proceed.

Just a little help

Thank You

Everybody

Pietro

0 Kudos
Reply
6,194 Views
FelipeGarcia
NXP Employee
NXP Employee

Hello Pietro,

 

I am very sorry for my late reply. We have been under a big workload and we have many questions on the queue.

 

Unfortunately, in in mcu-boot for FRDM-K64F there is no MSD bootloader example. However, I recommend you to check the community document below. This bootloader was implemented for IAR IDE.

 

https://community.nxp.com/docs/DOC-102629 

 

If you want to learn more about MCUXpresso IDE I recommend you to watch the following videos.

 

MCUXpresso IDE - Introduction Video

MCUXpresso IDE - Importing SDK Libraries

MCUXpresso IDE - Creating a new SDK Project

MCUXpresso IDE - Importing an SDK Example Project

MCUXpresso IDE - Using LPCOpen Examples

MCUXpresso IDE - Project Settings

 

Hope it helps!

 

Best regards,

Felipe

6,193 Views
pietrodicastri
Senior Contributor II

Ok Thank You.

I am trying to understand trying and trying,,

It could be useful to have in the SDK a bootloader using the MSD.

Thank You

Pietrp

0 Kudos
Reply
6,193 Views
pietrodicastri
Senior Contributor II

Hi Felipe

I have imported a project with the KDS  from an older SDK version. With the help of the running project on KDS I was able to produce by hand a running project with a MSD. My last goal is to produce a bootloader. I need to know how to intercept the communication for handling the file data to write in the flash. So I need the phisical format the data are vehiculated and a way to hang the host while the data are written in the flash to avoid the loss of data.

If You can inform me how to get these information it would be great.

Still how to import a project with the MCUXpresso is an open question and please help also on that front.

Thank you

Pietro

0 Kudos
Reply
6,193 Views
pietrodicastri
Senior Contributor II

Hi

I am desperately trying to import a project in MCUXpresso,

Nothing works.

I have not any SDKs installed. If I press the button for importing from the web the request hang forever.

I tried to build the USB_ramdisk by hand importing the files by hand but I do not finalize, without the definitions

properly in place.

Please give me a consistent way to use the importing of a project.

Pietro

0 Kudos
Reply
6,193 Views
pietrodicastri
Senior Contributor II

Hi Felipe

I have downloaded the SDK

int the directory \SDK_2.7.0_FRDM-K64F\docs\mcu-boot

I see the bootloader is not supported for storage device style.

Simply you need to download with a tool.

in the directory

SDK_2.7.0_FRDM-K64F\middleware\mcu-boot\src\bootloader

 I see some sources for the bootloader. So these sources are not supportig the

MSD for bootloading, it is necessary to add the support. Is it correct???

Thank You

Pietro

0 Kudos
Reply
6,193 Views
pietrodicastri
Senior Contributor II

Hi Felipe

I am trying to follow the suggestions in

USB MSC device bootloader revision for FRDM-KL25Z (IAR) 

I think with MCUXpresso I will go nowhere. Too many things are out of place.

I will need to fit for now on the FRDMK64

Is the project ready to run in the mcu-boot ???

Give me a valid suggestion to have something already running...

Thank You

Pietro

0 Kudos
Reply
6,193 Views
pietrodicastri
Senior Contributor II

Thank You Felipe

I am happy to have these references now.

There is something I need to understand clearly.

1 ) If the board works as a device a PC is necessary to send the code as writing to the disk

2) If the board is a host, when a disk is pluggedn in the USB board it will automathically take the file in without actions.

Is it correct???

Now at a glance I would like to have a starting point for building a bootloader with the MCUXpresso.

Is there a project ready to run? I am trying but I do navigate in the mcu-boot and I not find it. If it is necessary to build by hand it is ok.
Tell me the best documentation to build this project.

Thank You

Very much

Pietro

0 Kudos
Reply
6,193 Views
pietrodicastri
Senior Contributor II

Does any assistance exists?

I am stryggling to find out where the bootloader is here...

Pietro

0 Kudos
Reply
6,193 Views
FelipeGarcia
NXP Employee
NXP Employee

Hello Pietro,

 

I am sorry for the late reply. The main difference between these app notes is that one bootloader works as USB host and the other as device. This means that host will wait for a USB stick to be plugged into the board and the device enumerates as a MSD in the PC.

 

As you can see, these application notes are really old. The most recent software is located in the below links.

AN4368: https://www.nxp.com/webapp/Download?colCode=AN4368SW 

 

AN4379: USB MSC device bootloader revision for FRDM-KL25Z (IAR)

 

However, if you like to use the latest bootloader software we have available I highly recommend you to check the examples we have included in the MCUXpresso SDK, this will depend on the MCU you are working on.

 

You can download the SDK in the following link. Please make sure you add mcu-boot middleware before downloading the SDK package.

 

Welcome | MCUXpresso SDK Builder

 

Hope it helps!

 

Best regards,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored.

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------ 

6,193 Views
pietrodicastri
Senior Contributor II

Hello

It is just a simple question.

Hopefully it is coming,,,

Pietro

0 Kudos
Reply