need support for S32V234 EVB2 linux kernel sources code set up on our PC(locally)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

need support for S32V234 EVB2 linux kernel sources code set up on our PC(locally)

2,733 次查看
vaibhav_n
Contributor I

Hello,

We are using S32V234-EVB2- SC29288, and wanted to set up LINUX KERNEL 4.19. version locally.

Please do provide documents to set up kernel source code base locally. i.e complete kernel sources, including all drivers sources, that can be modified/build image with modified kernel sources.

This is to add custom drivers and modify existng drivers in kernel.

Thanks.

0 项奖励
回复
1 回复

2,659 次查看
paulvlase
NXP Employee
NXP Employee

Hello [email protected]‌

 

This community space do not cover the topic you need assistance on.

Please create new NXP support case according to following procedure:https://community.nxp.com/docs/DOC-329745

I think you can find more info about Linux BSP build procedure here.

Hope this helps,

Paul

0 项奖励
回复