What's the difference between "S32 Design Studio for Power Architecture v1.1 " and "S32 Design Studio for Power Architecture Version 2017.R1"?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What's the difference between "S32 Design Studio for Power Architecture v1.1 " and "S32 Design Studio for Power Architecture Version 2017.R1"?

3,088件の閲覧回数
pingfang
Contributor III

Hi.

What's the difference between "S32 Design Studio for Power Architecture v1.1 " and  "S32 Design Studio for Power Architecture Version 2017.R1"?

If I use S32R274 , do both of these can be used ?

Thank you.

タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,804件の閲覧回数
pingfang
Contributor III

Thank you ,Daniel.

0 件の賞賛
返信

2,804件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hello, 

2017.R1 is the latest version of the S32 Design Studio for PA. The release notes can be found here: S32 Design Studio for Power Architecture 2017.R1 (Windows/Linux) released! 

My personal advice is to use the 2017.R1 since it contains an updated GCC version compared with the older version v1.1

In regards with your main question: 

If I use S32R274 , do both of these can be used ?

The answer is Yes - both versions supports the S32R274.

Hope this helps!

Daniel

0 件の賞賛
返信