Radar FFT processing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Radar FFT processing

3,271件の閲覧回数
olivierdoare
NXP Employee
NXP Employee

What is the number of points used to perform the range_FFT the doppler_FFT and the reason why you need this number of points

regards,

Olivier

0 件の賞賛
返信
1 返信

2,824件の閲覧回数
iulianbulancea
NXP Employee
NXP Employee

Hi Olivier,

In the example shown Accelerate the Discrete Fourier Transform with NXP SPT  the number of points used for Range FFT is M=512 and for Doppler FFT is N=256, which means that one frame has N=256 chirps, and each chirp has M=512 samples.

In order to perform the FFT algorithm, the number of points (M and N) must be a power of 2. In general, the larger number the better the resolution.

Regards,

Iulian

0 件の賞賛
返信