RDK-Demo Controller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RDK-Demo Controller

8,771件の閲覧回数
burak_
Contributor II

Hi,

I have installed RDK-demo controller on my windows 10 laptop. But when ı try to run program, nothing happens. Program window does not open. In task manager, the task is running. I tried to run it as administrator, nothing has changed. Who can help me solving this issue?

0 件の賞賛
返信
5 返答(返信)

7,589件の閲覧回数
Iktler
Contributor I

Are there any new solutions? I had exactly the same problem...

0 件の賞賛
返信

8,754件の閲覧回数
longfeiwang
Contributor III

Do you mean it can't be programmed? Or it doesn't run after programming?

0 件の賞賛
返信

8,750件の閲覧回数
burak_
Contributor II

I mean, I cannot open the GUI. When ı double click on icon, the application does not open but it is running on background, ı can see in task manager.

0 件の賞賛
返信

8,748件の閲覧回数
longfeiwang
Contributor III

You need to install the correct version of the matlab runtime environment and set the correct TFTP directory, then you can run app.exe normally.

0 件の賞賛
返信

8,719件の閲覧回数
marmar
Contributor I

I have the same problem. Where should I set the right TFTP directory?

0 件の賞賛
返信