Linux Embedded Challenge ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux Embedded Challenge Knowledge Base

ディスカッション

ソート順:
Presentation for the first workshop session. A training on how to connect to UDOO and run Android apps.
記事全体を表示
Embedded Linux Conference Pass LinuxCon Europe is the place to learn from the best and the brightest, delivering content from the leading maintainers, developers and project leads in the Linux community and from around the world. There's simply no other event in Europe where developers, sys admins, architects and all types and levels of technical talent gather together under one roof for education, collaboration and problem-solving to further the Linux platform.  Who Attends: Developers - Software Developers, Programmers, Core Maintainers and Linux IT Professionals Operations - IT Operations Experts, System Administrators and Chief Architects Business & Legal - Corporate End Users, Senior Business Executives, Legal Counsel Plus Students, Media, Analysts and other professionals with an interest in the Linux ecosystem Kindle Voyage The Kindle Voyage is Amazon’s latest e-reader, but instead of being value-focused, the Voyage is a high-quality device with a crisper screen and fancy, squeezable touch buttons. Specifications Screen: 6in e-paper (300ppi) Dimensions: 162 x 115 x 7.6 mm Weight: 180g (3G version 188g) Connectivity: Wi-Fi (3G optional) Storage: 4GB Battery life: rated for approximately 21 hours of reading Source: www.theguardian.com ​ Garmin Forerunner 10 The Garmin Forerunner® 10   GPS watch, powered by Freescale technology, tracks distance, pace and   calories at the press of a button, enabling runners to enjoy the benefits of   a sophisticated GPS watch without the bulk.
記事全体を表示
We installed our usb wireless adapter (tp-link tl-wn722n) on the board and we were able to connect to wi-fi networks through it and through the board with the help of the web interface. Then we installed the package udoo-softap and after a restart we could connect to the default named udoo-hotspot network (we did not change anything in the config file just pointed the daemon to the aforementioned config file). We could connect to the network but it had no internet access because our usb adapter was displayed as not ready when we tried to debug (work in progress).
記事全体を表示
A house model with strategically placed sensors.
記事全体を表示
In acest clip video va prezentam posibila schema a apartamentului , acesata schema poate suferii modificari in functie de evolutia proiectului.
記事全体を表示
Project Presentations & Grading Rules
記事全体を表示
Registration requirements Minimum skills Previous experience with C or Java is needed. Previous experience with Linux systems is needed. Experience with embedded programming is a PLUS but not a MUST. Team one to three members from either Politechnica University of Bucharest or Military Technical Academy. Judging Criteria Originality Is this something new or improving something that existed before ? Execution Does it do what it should do, are there any major issues ? Usability Is the project easy to use and/or integrate ? Utility Does it have applicability within the Automotive domain ?
記事全体を表示
Wandboard Each selected team for Linux Embedded Challenge will receive a Wandboard Quad Core board which will be used as hardware platform for its project. Quick start guide User manual Processor details Wandboard enclode assembly guide Linux Git repo: https://www.github.com/wandboard-org/linux For more details, visit http://www.wandboard.org/.
記事全体を表示
Aceasta esta macheta noastra . o sa adaugam mai multi senzori, metoda de autentificare ,leduri  
記事全体を表示
- am stabilit conexiunea intre senzorul IR si placa UDOO - am facut un program relativ simplu pentru a putea afisa masuratorile efectuate de catre senzor Se observa si in video ca masuratoarea nu era una fixa deoarece colegul micsorea/marea raza de actiune a senzorului. Din pacate senzorul are o eroare de masurare de aproximativ +/-2 per masuratoare atunci cand distanta de masurare a senzorului nu se modifica. (furca blocata)
記事全体を表示
If you are willing to learn new technologies, use open-source software and promote your novel ideas about Linux, Automotive and Embedded, Linux Embedded Challenge is your opportunity to amaze everybody. Form your team (1-3 members) and research a project idea related to Automotive which can be realized using Freescale Linux BSP and platform. Challenge yourself and enroll to Linux Embedded Challenge by sending an e-mail at [email protected]. The format of the e-mail is: Subject: [LinuxEmbbededChallenge] [TEAMNAME] Project Name Team Description Project Description: Describe your idea in detail Include architectural diagrams and  used technologies Mention the improvements it brings to Automotive world. Please send you submissions in English. Enrollment period:  1 - 20 June, 2014. Extended Enrollment Period:  1 June - 4 July, 2014.
記事全体を表示
IoT presentation
記事全体を表示
The attached archive contains the starting point for developing an OpenVG-based embedded graphics application on the Wandboard. It contains 2 items: 1) The training presentation:      These are the support slides for the OpenVG presentation held during the Linux Embedded Challenge workshop. 2) The support application:      This is a sample application meant to aid in setting up the platform for an OpenVG-based application.      In order to compile it directly on the Wandboard, you will need the arm-linux-gnueabi-g++ compiler. If it is not already installed on the board, you can obtain it by installing the g++-arm-linux-gnueabi package:      sudo apt-get install g++-arm-linux-gnueabi      Use the provided Makefile to build the application. It provides an example on how to: Set up the platform (using X11) and the EGL objects (context, rendering surface etc.) Create an OpenVG path Create a linear gradient paint Create a pattern paint based on a user-generated image Fill and stroke a path Use transformation matrices to scale, rotate and translate a rendered object  
記事全体を表示
Aici demonstram legatura dintre semnalul preluat de la volanul pentru jocuri video si servomotoarele care controleaza farurile. Volanul este conectat prin USB, iar semnalul este preluat in procesorul Cortex A9. Este prelucrat si transmis catre coprocesorul M4 prin interfata seriala, de unde sunt actionate motoarele. De asemenea, am refacut modelul de bot de masina, care are acum un design mai realist.
記事全体を表示
Assembly of our project using 2 servo motors, the Udoo board, and a separate voltage regulator for the power for the servo's.  We probably did something wrong. one of the servos is dead ( it seems the inside gears are damaged, we can hear it spinning, but it doesn't move on the outside. We are using cheap, plastic gears in the servo).
記事全体を表示