Linux Embedded Challenge Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linux Embedded Challenge Knowledge Base

Discussions

Sort by:
Aplicatia administrativa a bazei de date. Design-ul este inca primar deoarece sunt singur in echipa si nu am apucat sa fac si design-ul dar core-ul merge. Pentru cine vrea sa vada cum merge cu mana lui: Adresa: catalin.etrandafir.ro Cont administrator: username - admin parola - admin Daca se buguieste puteti sa puneti un comentariu :smileygrin:
View full article
-we implemented the page where you can get access based on the QR code information, you get a message if the access is granted or denied, if someone enters the field, the admin will receive a notification in logs platform. -if the request time doesn't match the current time, administrator will receive a notification in the admin logs platform that will inform why the access was denied. -exact hour and data are displayed on the page.
View full article
The video summarizes the functionality of web server running on the UDOONeo board and a web interface. Connecting through ssh, we can see the feedback that the server is giving. From the web interface, the user has access to the following functionalities: - put the device in learning mode (giving two names - for the device and for the command which are being learn) - select an already learnt command, having the possibility to schedule it for a further use or directly trigger it. The video also shows the feedback given by the server while running and communicating with the web interface.
View full article
In acest filmulet prezentam indeplinirea sarcinilor corespunzatoare primei etape: conectarea senzorilor la placa UDOO.citirea senzorilor(temperatura, umiditate, altitudine, presiune atmosferica si intensitate luminoasa) si afisarea datelor in terminalul Linux. De asemenea, se poate observa ca folosim si un LED care semnalizeaza nivelul de lumina(se aprinde atunci cand nivelul intensitatii scade sub o anumita valoare). Prima parte a filmuletului prezinta realizarea conexiunilor cu placa . Toti senzorii sunt alimentati de la 3.3V conform specificatiilor pentru functionare optima din foile lor de catalog. Totodata, aceasta tensiune este sub pragul de 3.3V ceea ce protejeaza porturile de intrare ale placutei. Conexiunea fizica UDOO - calculator a fost realizata prin USB iar pentru a avea acces la terminal s-a folosit VNC + Putty In partea doua a doua a filmuletului se observa afisarea in consola a datelor citite de la senzori, iar ultima parte reprezinta un bonus prin care dorim sa semnalizam scaderea intensitatii luminoase sub un anumit prag prin aprinderea unei lumini, in cazul de fata un LED.
View full article
Our project is Adaptive Cruise Control and for our first milestone we built a proof-of-concept automobile which can be controlled from a computer with the help of an application. In this app the speed can be adjusted and the car can be controlled using the WASD keys. Also, it has the option of cruise control which moves the car forward at a constant speed.
View full article
Milestone_1 Implementarea hardware si software; Aplicatia grafica a sistemului: ofera o vedere top-down a intersectiilor si a celor 2 vehicule; Posibilitatea de a alege punctul de start si punctul de oprire a vehiculelor; Vehiculele incetinesc cand se apropie unul de celalalt pentru a evita coliziunea.
View full article
Aici demonstram legatura dintre semnalul preluat de la volanul pentru jocuri video si servomotoarele care controleaza farurile. Volanul este conectat prin USB, iar semnalul este preluat in procesorul Cortex A9. Este prelucrat si transmis catre coprocesorul M4 prin interfata seriala, de unde sunt actionate motoarele. De asemenea, am refacut modelul de bot de masina, care are acum un design mai realist.
View full article
Site-ul meu catalin.etrandafir.ro redirectioneaza catre adresa router-ului meu pe un port care redirectioneaza spre placuta UDOO pe portul serverului Tomcat. Daca serverul e pornit oricine care va intra pe catalin.etrandafir.ro va putea folosi aplicatia.
View full article
In this video, you are able to see the running mode of a python sketch that we used to introduce data from our sensors in a database every 10 seconds, the database itself and the web page which shows both the information stored in the database in a fancy format (the last entry, refresh every 15 seconds) and also 3 charts that describe the evolution of temperature, humidity and pressure over time.
View full article
Buna ziua, Pentru primul milestone am conectat o pereche laser-fotorezistor la plăcuța UDOO și am citit valorile analogice (simuland inaltimea produsului final). Multumesc!
View full article
   În urma masuratorilor am constatat ca pompele trag 50ml de apa intr-un timp de 8.5sec, prin urmare in 34sec in pahar au ajuns 200ml de apa.    Timpii activarii fiecarei pompe pentru intervalul dorit au fost preluati din memoria nevolatila (fisier creat pentru milestone 1) si transmisi procesorului de Arduino.    Acesta din urma a comandat motoarele prin intermediul releelor.
View full article
Am conectat la placa UDOO o pereche dioda laser - fotorezistor si un accelerometru si putem efectua citirile necesare proiectului.
View full article
   Realizarea primului milestone presupune realizarea interfetei web, care sa contina atat butoane pentru controlul robotului, cat si o fereastra de feedback de la acesta. Interfata este structurata astfel incat sa contina blocuri pentru: - status-ul de conectare; - live streaming; - feedback de la robot; - controlul robotului de la distanta.    Pentru realizarea interfetei si a comuncarii dintre interfata si Arduino, au fost necesare urmatoarele fisiere: - server.py (programul aflat in acest fisier este responsabil pentru crearea webserver-ului); - serialworker.py; - main.js; - index.html; - css.css; - serial2ws.ino.  
View full article
Pentru aceasta etapa am implementat o aplicatie in python, folosind opencv, prin intermediul careia calculam distanta de la camera la obiectul nostru. Am considerat numarul masinii din fata ca fiind un dreptunghi verde. Metoda pe care o folosim pentru a calcula distanta pana la obiect se bazeaza pe asemanarea triunghiurilor, iar formula pe care am implementat-o este: D = (W x F) / P W: latime obiect F: distanta focala P: latimea perceputa de camera P.S. Cand am masurat pentru 60 cm, initial masura bine dar apoi telefonul a intrat in cadru si camera a detectat un contur mai mic, de aceea nu este foarte exact.
View full article
Am construit cadrul harpei, am montat diodele laser (alimetate de baterii, cu un intrerupator) si am montat si realizat si circuitul cu fotorezistoare.
View full article
- we built our robot and as you can see we printed a bridge beetwen the motors with our 3D printer - we have already bought a very good battery but it has not arrived yet, we are sorry for this - our robot is functional and we chose firstly to give commands throw udoo command line with .ino files, but in the next Milestone we will change this because we realised that it would be much better to command throw web server
View full article
Assembly of our project using 2 servo motors, the Udoo board, and a separate voltage regulator for the power for the servo's.  We probably did something wrong. one of the servos is dead ( it seems the inside gears are damaged, we can hear it spinning, but it doesn't move on the outside. We are using cheap, plastic gears in the servo).
View full article
The robot is assembled and powered from battery. User is able to command the robot wheels from the web interface.
View full article
Am instalat Tomcat 8.5.14 si MySQL server 5.5 pe placuta UdooNeo, apoi am realizat o aplicatie web in Tomcat care sa faca legatura intre o interfata grafica in browser accesabila de catre utilizator si baza de date. Utilizatorul poate cere in request pentru o anumita data, ora si durata iar daca nu mai exista in request in acea perioada de timp utilizatorul primeste in cod pe care il poate folosi pentru a accesa serverul in perioada de timp ceruta.
View full article
am implementat grafica 3D serverul de pe placuta controleaza pozitia,directia si comportamentul masinii.
View full article