WillyFog_Milestone_1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WillyFog_Milestone_1

WillyFog_Milestone_1

The video summarizes the functionality of web server running on the UDOONeo board and
a web interface. Connecting through ssh, we can see the feedback that the server is giving.

From the web interface, the user has access to the following functionalities:
- put the device in learning mode (giving two names - for the device and for the command which
are being learn)
- select an already learnt command, having the possibility to schedule it for a further use or
directly trigger it.

The video also shows the feedback given by the server while running and communicating
with the web interface.

(view in My Videos)
Labels (1)
No ratings
Version history
Last update:
‎05-07-2017 09:49 AM
Updated by: