using LX2160A-RDB Reference Board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

using LX2160A-RDB Reference Board

2,589 次查看
16624486
Contributor I

If using LX2160A-RDB Reference Board, should we need to connect codeWarrrior@TAP to the LX2160A-RDB for system debug ? 

标记 (1)
0 项奖励
回复
3 回复数

2,474 次查看
16624486
Contributor I

I mean, how to use the LX2160A-RDB reference board?

Should we need to use the simulator(code Warrior@TAP) to connect the computer to  LX2160-RDB to evaluate LX2160A?

or just need the other cable to connect the computer to LX2160-RDB? 

0 项奖励
回复

2,474 次查看
ufedor
NXP Employee
NXP Employee

The board is provided fully operational, with latest NXP LSDK firmware installed.

The DB9 shielded serial cable (to connect console to the host PC) is included in the RDB kit.

Pre-built firmware images can be programmed by means of U-Boot using Ethernet (Cat-6 Ethernet cable is included) TFTP to transfer them from host PC.

Of course the CodeWarrior IDE, CodeWarrior TAP and Probe Tip are required for software debugging.

0 项奖励
回复

2,474 次查看
ufedor
NXP Employee
NXP Employee

Sorry, the request is not fully clear - please elaborate.

0 项奖励
回复