uart/serial problem with ls1046ardb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uart/serial problem with ls1046ardb

Jump to solution
1,995 Views
rans
Senior Contributor I

Hello,

 

We are using ls1046ardb, and the serial connection is received from console usb output.

The problem is that the serial does not work well (whether in Linux or uboot):

console shows the previous character so although a new character is pressed. It makes it really difficult to work with the serial. Doing ssh works just fine.

Thanks for any suggestion

0 Kudos
Reply
1 Solution
1,922 Views
rans
Senior Contributor I

I am using linux machine,

anyway, doing load unload module cdc_acm.ko or just PC reboot , solved the issue

View solution in original post

0 Kudos
Reply
2 Replies
1,946 Views
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

Are you using a windows host computer? 

0 Kudos
Reply
1,923 Views
rans
Senior Contributor I

I am using linux machine,

anyway, doing load unload module cdc_acm.ko or just PC reboot , solved the issue

0 Kudos
Reply