lsdk system reboot while kill -9 vpp&dpdk

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lsdk system reboot while kill -9 vpp&dpdk

1,671件の閲覧回数
nxppenpals
Contributor II

We have a custom board with LS2160 CPU on it.
Operating System: NXP LSDK 2004 main
Kernel: 4.19.90
.vpp version :vpp v22.06.1-release
dpdk version :DPDK 21.11.2
DPDK EAL init args: --huge-unlink --huge-dir /run/vpp/hugepages --no-pci --in-memory --no-telemetry --file-prefix vpp
restool -v
restool v2.4 (10.30.0 compatible)
restool -m
MC firmware version: 10.36.0
We run vpp include dpdk plugin on it
As a beginner ,we are dealing with a critical problem.
When we use kill -9 to force VPP to quit,
the system will reboot immediately without any crash logs.
Is there any way to solve the problem?
Thanks for advice from experienced experts.
Regards,

0 件の賞賛
返信
2 返答(返信)

1,649件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

1,639件の閲覧回数
nxppenpals
Contributor II

Thank you for your reply.
The ipsec feature is disabled in our vpp.
It seems that this bug can not cause system to  reboot.

0 件の賞賛
返信