We designed the PHY of SGMII using fiber port mode.
1. Do I need to add SFP to support fiber ports on the device tree? How to modify it?
2.Can the fiber port disable auto negotiation on ls1043.such as force 100Mbps?
Dear Hmc510,
you need to add the PHY, you have designed, to the device-tree, please use the next application note to get the details you need to know of it.
https://www.nxp.com/docs/en/application-note/AN5125.pdf
The port can't disable the auto negotiation.
From my point of view, It is not a good idea to disable auto-negotiation.