ls1046a using emmc as boot source

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ls1046a using emmc as boot source

1,759件の閲覧回数
shijj
Contributor I

hi

In  my coustom board,I use emmc/sd as boot source.but i don't use SDHC_CD_B pin.it always floating.my board is refer to ls1046ardb board.

Now I can boot from sd card ,but i can't boot from emmc.

why I can boot from sd? the SDHC_CD_B pin is floating  And Why I can't boot from emmc,Is it because PBL has special regulations for this pin?

in spec,when use sdhc as boot source, SDHC_CD_B pin be serve as the SDHC_CD_B pin for the eSDHC controller. This happens automatically when the microSD card is selected as the boot source for the board.

ラベル(1)
0 件の賞賛
返信
1 返信

1,652件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please provide the processor connection schematics as searchable PDF for inspection.

0 件の賞賛
返信