ls1046a using emmc as boot source

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ls1046a using emmc as boot source

1,237 次查看
shijj
Contributor I

hi

In  my coustom board,I use emmc/sd as boot source.but i don't use SDHC_CD_B pin.it always floating.my board is refer to ls1046ardb board.

Now I can boot from sd card ,but i can't boot from emmc.

why I can boot from sd? the SDHC_CD_B pin is floating  And Why I can't boot from emmc,Is it because PBL has special regulations for this pin?

in spec,when use sdhc as boot source, SDHC_CD_B pin be serve as the SDHC_CD_B pin for the eSDHC controller. This happens automatically when the microSD card is selected as the boot source for the board.

标签 (1)
0 项奖励
回复
1 回复

1,130 次查看
ufedor
NXP Employee
NXP Employee

Please provide the processor connection schematics as searchable PDF for inspection.

0 项奖励
回复