ls1046a: qman failure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ls1046a: qman failure

3,231件の閲覧回数
renaud
Contributor IV

We have a LS1046A based board with the following failure:

 

[    0.220387] fsl_dpaa_mac 1ae6000.ethernet: qman_init_fq(1951) = -5
[    0.302707] fsl_dpa dpaa-ethernet.0: qman_retire_fq(1951) = -22
[    0.373551] fsl_dpa dpaa-ethernet.0: qman_oos_fq(1951) = -22

 

Any idea what could be triggering this error during Linux boot (5.17). Can this be triggered by an hardware issue?

0 件の賞賛
返信
6 返答(返信)

3,123件の閲覧回数
renaud
Contributor IV

REturn result from MCR:

[ 0.213821] result = 0xf2
[ 0.245090] fsl_dpaa_mac 1ae6000.ethernet: qman_init_fq(1633) = -5
[ 0.326008] fsl_dpa dpaa-ethernet.0: qman_retire_fq(1633) = -22
[ 0.396850] fsl_dpa dpaa-ethernet.0: qman_oos_fq(1633) = -22

0 件の賞賛
返信

3,175件の閲覧回数
LFGP
NXP TechSupport
NXP TechSupport

could you please try with the NXP LLDP 6.1.36 it uses the LTS Kernel 6.1.

 

0 件の賞賛
返信

3,163件の閲覧回数
renaud
Contributor IV

Can you point me to the documentation to load the and build the distro?

0 件の賞賛
返信

3,145件の閲覧回数
LFGP
NXP TechSupport
NXP TechSupport
You will need to use the LLDP user guide, please follow to the next link to download the PDF file.
https://www.nxp.com/design/design-center/software/embedded-software/linux-software-and-development-t...
be sure to click in the PDF instead HTLM
0 件の賞賛
返信

3,211件の閲覧回数
LFGP
NXP TechSupport
NXP TechSupport

from my point view, the issue is not due to hardware.

It looks like you are trying to create a DPAA object before the DPAA drives be initialized.

 

0 件の賞賛
返信

3,190件の閲覧回数
renaud
Contributor IV

So we found that it happens on only on one for our boards. It does not happen after running a memory test from the boot loader, the difference being the pattern left in DDR memory - 0 with memory test, deadbeef when not run. 

We have not seen it happen on Linux 6.4.

Looking at the Linux log to see if there was anything that may have fixed the problem

 

 

0 件の賞賛
返信