ls1046a: qman failure

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ls1046a: qman failure

3,258 次查看
renaud
Contributor IV

We have a LS1046A based board with the following failure:

 

[    0.220387] fsl_dpaa_mac 1ae6000.ethernet: qman_init_fq(1951) = -5
[    0.302707] fsl_dpa dpaa-ethernet.0: qman_retire_fq(1951) = -22
[    0.373551] fsl_dpa dpaa-ethernet.0: qman_oos_fq(1951) = -22

 

Any idea what could be triggering this error during Linux boot (5.17). Can this be triggered by an hardware issue?

0 项奖励
回复
6 回复数

3,150 次查看
renaud
Contributor IV

REturn result from MCR:

[ 0.213821] result = 0xf2
[ 0.245090] fsl_dpaa_mac 1ae6000.ethernet: qman_init_fq(1633) = -5
[ 0.326008] fsl_dpa dpaa-ethernet.0: qman_retire_fq(1633) = -22
[ 0.396850] fsl_dpa dpaa-ethernet.0: qman_oos_fq(1633) = -22

0 项奖励
回复

3,202 次查看
LFGP
NXP TechSupport
NXP TechSupport

could you please try with the NXP LLDP 6.1.36 it uses the LTS Kernel 6.1.

 

0 项奖励
回复

3,190 次查看
renaud
Contributor IV

Can you point me to the documentation to load the and build the distro?

0 项奖励
回复

3,172 次查看
LFGP
NXP TechSupport
NXP TechSupport
You will need to use the LLDP user guide, please follow to the next link to download the PDF file.
https://www.nxp.com/design/design-center/software/embedded-software/linux-software-and-development-t...
be sure to click in the PDF instead HTLM
0 项奖励
回复

3,238 次查看
LFGP
NXP TechSupport
NXP TechSupport

from my point view, the issue is not due to hardware.

It looks like you are trying to create a DPAA object before the DPAA drives be initialized.

 

0 项奖励
回复

3,217 次查看
renaud
Contributor IV

So we found that it happens on only on one for our boards. It does not happen after running a memory test from the boot loader, the difference being the pattern left in DDR memory - 0 with memory test, deadbeef when not run. 

We have not seen it happen on Linux 6.4.

Looking at the Linux log to see if there was anything that may have fixed the problem

 

 

0 项奖励
回复