ls1028 openil emmc hs400 write error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ls1028 openil emmc hs400 write error

1,835件の閲覧回数
540915622
Contributor III

I use our own ls1028 board, the emmc model is the same as ls1028ardb.
When running OpenIL-1.10 version, emmc will report the following error when starting up.

 

 

[   27.306495] 000: mmc1: Got data interrupt 0x00600000 even though no data operation was in progress.
[   27.306502] 000: mmc1: sdhci: ============ SDHCI REGISTER DUMP ===========
[   27.306504] 000: mmc1: sdhci: Sys addr:  0x00000030 | Version:  0x00002202
[   27.306507] 000: mmc1: sdhci: Blk size:  0x00000200 | Blk cnt:  0x00000030
[   27.306509] 000: mmc1: sdhci: Argument:  0x00000000 | Trn mode: 0x00000033
[   27.306511] 000: mmc1: sdhci: Present:   0x01fd0008 | Host ctl: 0x00000034
[   27.306513] 000: mmc1: sdhci: Power:     0x00000006 | Blk gap:  0x00000000
[   27.306515] 000: mmc1: sdhci: Wake-up:   0x00000000 | Clock:    0x00000208
[   27.306517] 000: mmc1: sdhci: Timeout:   0x0000000c | Int stat: 0x00000001
[   27.306519] 000: mmc1: sdhci: Int enab:  0x037f100f | Sig enab: 0x037f100b
[   27.306521] 000: mmc1: sdhci: ACmd stat: 0x00000000 | Slot int: 0x00002202
[   27.306523] 000: mmc1: sdhci: Caps:      0x00fa0000 | Caps_1:   0x0000af00
[   27.306525] 000: mmc1: sdhci: Cmd:       0x00000c1a | Max curr: 0x00000000
[   27.306527] 000: mmc1: sdhci: Resp[0]:   0x00000b00 | Resp[1]:  0x0000000c
[   27.306529] 000: mmc1: sdhci: Resp[2]:   0x00000000 | Resp[3]:  0x00000000
[   27.306531] 000: mmc1: sdhci: Host ctl2: 0x00000081
[   27.306532] 000: mmc1: sdhci: ADMA Err:  0x00000000 | ADMA Ptr: 0xf81aa200
[   27.306534] 000: mmc1: sdhci: ============================================
[   27.364818] 001: mmc1: tuning execution failed: -110
[   27.420779] 001: mmc1: tuning execution failed: -110
[   27.476777] 001: mmc1: tuning execution failed: -110
[   27.532776] 001: mmc1: tuning execution failed: -110
[   27.672769] 000: mmc1: tuning execution failed: -110
[   27.728769] 000: mmc1: tuning execution failed: -110

 

 

emmc related information

 

 

[root@MYD-JLS1028 ~] # cat /mnt/mmc1/ios 
clock:          200000000 Hz
actual clock:   150000000 Hz
vdd:            21 (3.3 ~ 3.4 V)
bus mode:       2 (push-pull)
chip select:    0 (don't care)
power mode:     2 (on)
bus width:      3 (8 bits)
timing spec:    10 (mmc HS400)
signal voltage: 1 (1.80 V)
driver type:    0 (driver type B)

 

 

The following error is reported when writing

 

 

[root@MYD-JLS1028 ~] # dd if=/dev/zero of=/dev/mmcblk1 bs=500M count=1
[   45.896754] 001: mmc1: tuning execution failed: -110
[   45.952721] 001: mmc1: tuning execution failed: -110
[   46.008716] 001: mmc1: tuning execution failed: -110
[   46.064732] 001: mmc1: tuning execution failed: -110
[   46.120713] 001: mmc1: tuning execution failed: -110
[   46.176711] 001: mmc1: tuning execution failed: -110
[   46.232709] 001: mmc1: tuning execution failed: -110
[   46.288678] 001: mmc1: tuning execution failed: -110
[   46.344694] 001: mmc1: tuning execution failed: -110
[   46.400671] 001: mmc1: tuning execution failed: -110
[   46.456703] 001: mmc1: tuning execution failed: -110

 

 

When I use the LSDK-20.12 version to test, there will be no problems when writing emmc hs400 mode.
I copied the kernel Image compiled by LSDK-20.12 and directly copied it to the image of openil-1.10 to test and there would be no problems.

I wonder if there are some problems in hs400 mode of emmc driver of rt-linux.

0 件の賞賛
返信
1 返信

1,829件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please check whether the attached patches would be helpful.

0 件の賞賛
返信