ls1021a errata link

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ls1021a errata link

3,740 Views
renaud
Contributor IV

Cannot find the LS1021A errata documentation.

 

Could you give me a link?

Cheers.

0 Kudos
Reply
7 Replies

3,733 Views
ufedor
NXP Employee
NXP Employee

The processor Errata list is a confidential document.

0 Kudos
Reply

3,692 Views
renaud
Contributor IV

I cannot get to the link given to retrieve the document

0 Kudos
Reply

3,739 Views
renaud
Contributor IV

specially regarding the gianfar as I have difficulties to get it to work on Linux 5.11/14/16

0 Kudos
Reply

3,721 Views
renaud
Contributor IV

Also I found https://lore.kernel.org/all/[email protected]/

Does that mean you a 5.16 version working on tested on LS1021A-IOT?

0 Kudos
Reply

3,723 Views
renaud
Contributor IV

Note that I think I have applied the configuration to the AR8031 properly (disable smartEEE, set XTAL).

I can see packet being received and sometimes answers back from within the driver. That part bother me a lot. Why would a received packet arp request  not get a replay from the kernel all the time? 

0 Kudos
Reply

3,716 Views
ufedor
NXP Employee
NXP Employee

Received packet can be corrupted because of some issue on the interface between PHY and MAC.

0 Kudos
Reply

3,709 Views
renaud
Contributor IV

Are you saying that even with the checksum offload feature, the packet will be passed to the driver even if corrupted?

There is one instance when the FSL_GIANFAR_DEV_HAS_CSUM feature was disabled and saw arp request being replied. I have not been able to repeat it.

0 Kudos
Reply