ls1021a errata link

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ls1021a errata link

3,753件の閲覧回数
renaud
Contributor IV

Cannot find the LS1021A errata documentation.

 

Could you give me a link?

Cheers.

0 件の賞賛
返信
7 返答(返信)

3,746件の閲覧回数
ufedor
NXP Employee
NXP Employee

The processor Errata list is a confidential document.

0 件の賞賛
返信

3,705件の閲覧回数
renaud
Contributor IV

I cannot get to the link given to retrieve the document

0 件の賞賛
返信

3,752件の閲覧回数
renaud
Contributor IV

specially regarding the gianfar as I have difficulties to get it to work on Linux 5.11/14/16

0 件の賞賛
返信

3,734件の閲覧回数
renaud
Contributor IV

Also I found https://lore.kernel.org/all/[email protected]/

Does that mean you a 5.16 version working on tested on LS1021A-IOT?

0 件の賞賛
返信

3,736件の閲覧回数
renaud
Contributor IV

Note that I think I have applied the configuration to the AR8031 properly (disable smartEEE, set XTAL).

I can see packet being received and sometimes answers back from within the driver. That part bother me a lot. Why would a received packet arp request  not get a replay from the kernel all the time? 

0 件の賞賛
返信

3,729件の閲覧回数
ufedor
NXP Employee
NXP Employee

Received packet can be corrupted because of some issue on the interface between PHY and MAC.

0 件の賞賛
返信

3,722件の閲覧回数
renaud
Contributor IV

Are you saying that even with the checksum offload feature, the packet will be passed to the driver even if corrupted?

There is one instance when the FSL_GIANFAR_DEV_HAS_CSUM feature was disabled and saw arp request being replied. I have not been able to repeat it.

0 件の賞賛
返信