ls1021a errata link

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ls1021a errata link

3,756 次查看
renaud
Contributor IV

Cannot find the LS1021A errata documentation.

 

Could you give me a link?

Cheers.

0 项奖励
回复
7 回复数

3,749 次查看
ufedor
NXP Employee
NXP Employee

The processor Errata list is a confidential document.

0 项奖励
回复

3,708 次查看
renaud
Contributor IV

I cannot get to the link given to retrieve the document

0 项奖励
回复

3,755 次查看
renaud
Contributor IV

specially regarding the gianfar as I have difficulties to get it to work on Linux 5.11/14/16

0 项奖励
回复

3,737 次查看
renaud
Contributor IV

Also I found https://lore.kernel.org/all/[email protected]/

Does that mean you a 5.16 version working on tested on LS1021A-IOT?

0 项奖励
回复

3,739 次查看
renaud
Contributor IV

Note that I think I have applied the configuration to the AR8031 properly (disable smartEEE, set XTAL).

I can see packet being received and sometimes answers back from within the driver. That part bother me a lot. Why would a received packet arp request  not get a replay from the kernel all the time? 

0 项奖励
回复

3,732 次查看
ufedor
NXP Employee
NXP Employee

Received packet can be corrupted because of some issue on the interface between PHY and MAC.

0 项奖励
回复

3,725 次查看
renaud
Contributor IV

Are you saying that even with the checksum offload feature, the packet will be passed to the driver even if corrupted?

There is one instance when the FSL_GIANFAR_DEV_HAS_CSUM feature was disabled and saw arp request being replied. I have not been able to repeat it.

0 项奖励
回复