ls1021a: Enhanced Optimization Register

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ls1021a: Enhanced Optimization Register

Jump to solution
826 Views
renaud
Contributor IV

Eventually got to start debugging our LS1021A based porotype.

it fails very early on writing to ddr->eor (0x108_0c00).

/* disable the re-ordering in DDRC */

ddr_out32(&ddr->eor, DDR_EOR_RD_REOD_DIS | DDR_EOR_WD_REOD_DIS);

I do not find a description of this register in the LS1021A manual Rev 3.1. 

I can access register sets such as DCFG, IFC but not the DDR controller. Though, it is not disabled as per DCFG_CCSR_DEVDISR5. My ls1021a-iot has not this problem.

 

Has anybody seen this issue?

 

 

0 Kudos
Reply
1 Solution
821 Views
renaud
Contributor IV

We did find the issue. The DDR reference clock was set to DDRCLK instead of DIFF SYSCLK. After that we had access to the DDR registers

View solution in original post

0 Kudos
Reply
1 Reply
822 Views
renaud
Contributor IV

We did find the issue. The DDR reference clock was set to DDRCLK instead of DIFF SYSCLK. After that we had access to the DDR registers

0 Kudos
Reply