linux pcie dts

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

linux pcie dts

5,528件の閲覧回数
shunpinglin
Contributor III

Now I have a problem about pcie dts. In ls1021a.dtsi, have a pcie description:

pcie@3400000 {
                        compatible = "fsl,ls1021a-pcie", "snps,dw-pcie";
                        reg = <0x00 0x03400000 0x0 0x00010000   /* controller registers */
                               0x40 0x00000000 0x0 0x00002000>; /* configuration space */
                        reg-names = "regs", "config";
                        interrupts = <GIC_SPI 181 IRQ_TYPE_LEVEL_HIGH>,
                                     <GIC_SPI 183 IRQ_TYPE_LEVEL_HIGH>; /* aer interrupt */
                        interrupt-names = "pme", "aer";
                        fsl,pcie-scfg = <&scfg 0>;
                        #address-cells = <3>;
                        #size-cells = <2>;
                        device_type = "pci";
                        num-lanes = <4>;
                        bus-range = <0x0 0xff>;
                        ranges = <0x81000000 0x0 0x00000000 0x40 0x00010000 0x0 0x00010000   /* downstream I/O */
                                  0x82000000 0x0 0x40000000 0x40 0x40000000 0x0 0x40000000>; /* non-prefetchable memory */
                        msi-parent = <&msi>;
                        #interrupt-cells = <1>;
                        interrupt-map-mask = <0 0 0 7>;
                        interrupt-map = <0000 0 0 1 &gic GIC_SPI 91  IRQ_TYPE_LEVEL_HIGH>,
                                        <0000 0 0 2 &gic GIC_SPI 188 IRQ_TYPE_LEVEL_HIGH>,
                                        <0000 0 0 3 &gic GIC_SPI 190 IRQ_TYPE_LEVEL_HIGH>,
                                        <0000 0 0 4 &gic GIC_SPI 192 IRQ_TYPE_LEVEL_HIGH>;
                };

                pcie@3500000 {
                        compatible = "fsl,ls1021a-pcie", "snps,dw-pcie";
                        reg = <0x00 0x03500000 0x0 0x00010000   /* controller registers */
                               0x48 0x00000000 0x0 0x00002000>; /* configuration space */
                        reg-names = "regs", "config";
                        interrupts = <GIC_SPI 182 IRQ_TYPE_LEVEL_HIGH>,
                                     <GIC_SPI 184 IRQ_TYPE_LEVEL_HIGH>; /* aer interrupt */
                        interrupt-names = "pme", "aer";
                        fsl,pcie-scfg = <&scfg 1>;
                        #address-cells = <3>;
                        #size-cells = <2>;
                        device_type = "pci";
                        num-lanes = <4>;
                        bus-range = <0x0 0xff>;
                        ranges = <0x81000000 0x0 0x00000000 0x48 0x00010000 0x0 0x00010000   /* downstream I/O */
                                  0x82000000 0x0 0x40000000 0x48 0x40000000 0x0 0x40000000>; /* non-prefetchable memory */
                        msi-parent = <&msi>;
                        #interrupt-cells = <1>;
                        interrupt-map-mask = <0 0 0 7>;
                        interrupt-map = <0000 0 0 1 &gic GIC_SPI 92  IRQ_TYPE_LEVEL_HIGH>,
                                        <0000 0 0 2 &gic GIC_SPI 189 IRQ_TYPE_LEVEL_HIGH>,
                                        <0000 0 0 3 &gic GIC_SPI 191 IRQ_TYPE_LEVEL_HIGH>,
                                        <0000 0 0 4 &gic GIC_SPI 193 IRQ_TYPE_LEVEL_HIGH>;
                };

In reg property, why does configuration space set 0x40 or 0x48? what's mean of the address of 0x40 or 0x48?

Please help! 

ラベル(1)
タグ(4)
0 件の賞賛
返信
2 返答(返信)

4,016件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

If you look from the root of the tree you can see that parent of these nodes has

#address-cells = <2>;

#size-cells = <2>;

So in the <reg> we need 4 32-bit values for single pair address : size on this bus. So each <reg> specifies that PCIe@340000 node occupies <0x0 0x00002000> = 0x2000 bytes at address <0x40 0x00000000> = 0x4000000000 while the second PCIe occupies 0x2000 bytes at address 0x4800000000. The same PCIe@340000  <range> refers to the addresses <0x40 0x40000000> = 0x4040000000 and 0x4000010000 , while PCIe@350000  <range> refers to the addresses 0x4840000000 and  0x4800010000 

 It is in accordance to the LS1021A memory map. The LS1021A reference manual table 2-1 shows

pastedImage_1.png

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,016件の閲覧回数
shunpinglin
Contributor III

Now I understand these. Thank you very much!

0 件の賞賛
返信