lib path for ls1043ardb

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lib path for ls1043ardb

825件の閲覧回数
dibyarekha
Contributor IV

Hi Team,

 

I am using ls1043ardb, I want to compile my application program. I am following LSDKYOCTOUG.pdf , I want to know the lib path in the build_ls1043ardb folder. In my Makefile I want to mention the lib path

Please let me know

I have found the path at build_ls1043ardb/tmp/work/ls1043ardb-fsl-linux/fsl-image-mfgtool/1.0-r0/recipe-sysroot/usr/lib

is this correct path?  if No, Please tell me the correct path

if I am using this path, while cross-compiling I am getting library linking error.

It is searching the libraries in /usr/lib path.

Or I am using wrong toolchain for cross-compiling

if the toolchain problem is there please tell me which toolchain I should use

Please help me in solving the issue

 

 

Following are the errors

/opt/fsl-qoriq/3.1/sysroots/x86_64-fslsdk-linux/usr/libexec/aarch64-fsl-linux/gcc/aarch64-fsl-linux/9.3.0/real-ld: cannot find /usr/lib/libc.so.6
/opt/fsl-qoriq/3.1/sysroots/x86_64-fslsdk-linux/usr/libexec/aarch64-fsl-linux/gcc/aarch64-fsl-linux/9.3.0/real-ld: cannot find /usr/lib/libc_nonshared.a
/opt/fsl-qoriq/3.1/sysroots/x86_64-fslsdk-linux/usr/libexec/aarch64-fsl-linux/gcc/aarch64-fsl-linux/9.3.0/real-ld: cannot find /usr/lib/ld-linux-aarch64.so.1

 

I am using net-snmp in my application code

0 件の賞賛
返信
0 返答(返信)